ST-Link/V3 MINIE not connecting to H723 via CubeProgrammer
Hi,
I had been using ST/Link 2.1 nucleo header so far to program and debug custom STM32 H723 ZG boards and wanted to switch to ST/Link v3 in order to debug with compact probes. Thus I ordered two genuine ST-Link/V3 MINIE from Mouser.
My custom board and debug connector is confirmed to be working since I can connect and program with STLink V2 and V2.1 .
I've tried to connect through CN2 B2B connector as well a CN4 STDC14 Connector but I can not connect to the target via either method on both MINIE board I purchased.
I've updated firmware to V3J10M3, tried versions with and without Mass Storage. I've tried all Modes and Reset Modes.
Still I can not get target informations. Interestingly, CubeProgrammer states that the (target ?) voltage is 0.24V.
Wondering if there is an issue with my custom STD14 to JST-SH6 cable, i've tried to use a V3-SET with the very same cable and I can successfully connect to the MCU. Displayed voltage is 0.0V which is surprising because I get 3.25V with ST-Link V2.
My custom debug connector was designed for ST-Links V2s and only have a 5V input pad instead of 3.3v. So I can't power the board from the ST/Link. But since I power my board from an external USB, that shouldn't be an issue with the ST/Link V3 MINIE. Unless I am missing something.
Could there be a GND reference sharing problem ? The USB GND and Debug Connector GND are shared in my board routing. And anyway, I'd expect that the GND is shared though the computer USB hub as well.
Any idea why the genuine ST-Link/V3-MINIE are not working ??
Do you know what is and how is calculated the (target) voltage displayed by openocd when connecting to a St-Link ?