Skip to main content
Associate
December 9, 2023
Question

ST_Link V3MINI and Cube programmer

  • December 9, 2023
  • 3 replies
  • 1219 views

Dear mr.

I'm having problems with my project,

Everything was working fine, but one morning I lost connection with the target unit, see attached image.

I tried this with:

  Two ST_Link V3MINI (I got them directly from ST)

  Three different target board STM32G071 and STM32G030.

  Two different PCs.

   Two USB cable.

   Uninstall and install SW from ST.

My configuration is no RST wire.

One of the questions- My setting is "Soft reset" but in the log I see "HWrst reset mode".

I don't remember... maybe the problem started after the ST-Link update?

Please advise.

Regards

This topic has been closed for replies.

3 replies

Technical Moderator
December 11, 2023

Hello @Micisag,

Make sure to use latest release of STM32CubeProgrammer (2.15).

Then, please keep me informed about your result.

Imen

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
MicisagAuthor
Associate
December 12, 2023

Hello Imen,

My target board STM32G071 start working after I've move USB cable from front my PC to rear(direct to MB of the PC)

Target board STM32G030 stay not working,

Yes, I've use latest STM32CubeProgrammer and ST-link FW.

Regards,

Micisag

Technical Moderator
December 12, 2023

Try connecting the reset pin and connect under reset mode!

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"