Skip to main content
J.Christ
Associate II
June 16, 2025
Question

STM32 Cube Programmer Custom Loader Not Found causing error

  • June 16, 2025
  • 4 replies
  • 573 views

We have a custom loader from one of our boards.  It is working in STM32 Cube MX Prog V2.16 but when I launch V2.19 and try to connect to a unrelated boards I get this error:

JChrist_0-1750113584289.png

The error is understandable because the path to the loaders is incorrect.  The issue is I never told V2.19 to use this external loader and it doesn't even show up in the list of available loaders.  It some how figured out that I have used this loader in the past (but it didn't quite figure out the correct location of the loader) and for some reason it is trying to access it.  I mess with loaders so infrequently I have no idea how to fix this issue.

The custom loader does show up in V2.16 and doesn't produce this error:

JChrist_1-1750113873860.png

 

Suggestions?

 

Jacob

4 replies

Technical Moderator
June 18, 2025

Hello @J.Christ ,

What is your hardware board ? Is it a Nucleo or custom board? 

Does have any protections enabled? If yes, try disable the read protection.

Maybe you have the same issue as this thread: Solved: STM32CubeProgrammer cannot connect to MCU

 

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
MRech.1
Associate II
October 14, 2025
Aziz BRIGUI
Technical Moderator
October 14, 2025

Hello,

That's because the loader value is cached (For all versions). To workaround this:

1- Close CubeProgrammer

2- Go to "C:\Users\[YOUR_USER_NAME]\STMicroelectronics\STM32CubeProgrammer" and delete "config.properties" file

3- Reopen STM32CubeProgrammer.

PS: If you're on Linux, the path is "/home/[YOUR_USER_NAME]/.STM32CubeProgrammer"

You should no longer have the pop-up.

Hope this helps,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MRech.1
Associate II
October 14, 2025

Thanks Aziz. Unfortunately deleting this file does not help (on Linux it is located at /home/[user]/.STM32CubeProgrammer/config.properties)