STM32CubeProgrammer 2.10.0 and 2.11.0 External loader bug: if the EL's filename has more tha one dot (one dot only for its extension name) STM32CubeProgrammer goes in error.
If the name (filename) of module has more than one dot ( "." ) the STM32CubeProgrammer can list it in the external loder (EL) selection, but when STM32CubeProgrammer tries to use the module it fails (it generates an error).
For example this EL name generates the error: EN25Q40_MT447R2_2.0.0.stldr
the same file renamed into EN25Q40_MT447R2.stldr (removing all dots) works.