STM32CubeProgrammer 2.11.0 released
New features
• Tool updater: can be used to upgrade STM32CubeProg from v2.10.0 to v2.11.0 for all supported operating systems (Windows®, Linux®, and macOS®)
• SFI: – SFIx support for STM32U585xx microcontrollers via SWD/JTAG – New SFI/SFIx graphical user interface (GUI) – STM32 Trusted Package Creator SFI GUI enhancement – Support for integrity check with the STM32H7 Series and STM32U5 Series microcontrollers • STM32U5 Series: the GUI supports the RDP regression with password
• New bootloader support for STM32L476xx microcontrollers
• STM32MP13xx microprocessors: – Flash memory load via USB-DFU/UART – SSP (command-line interface only) – OTP: CLI/GUI
Fixed issues
90858 [STM32WB][CLI] Optimize FUS, STACK, and USER app upgrading automatically. 104409 STM32H735xx: SFI is very slow over SWD.
109240 Extra option bytes displayed for STM32G030C6: PCROP1A_STRT, PCROP1A_END, PCROP1A_RDP, PCROP1B_STRT, PCROP1B_END, and BOOT_LOCK, SEC_SIZE.
110205 Fix the reading of CHIPID (DBGMCU_DBG_AUTH_DEVICE) on STM32U5 microcontrollers.
110614 [CLI] Error level not reported correctly for the CRC safety feature using STM32CubeProgrammer_CLI.
117163 Launch problem when running the STM32CubeProgrammer GUI from another path.
119604 [STM32G0][OB] Sector erase cannot be achieved and an STM32CubeIDE debug error occurs when nSWAP_BANK=0.
120935 STPC v2.9 cannot generate a correct .sfi file for SFI.
121452 [OB] Incorrect SRAM2b secure address for STM32WB1xxx.
121713 Typo: “Memory & file edition�?.
123018 [STM32H7][CM4] BOOT_CM4_ADD cannot be modified.
123740 [DFU] The single-bank configuration is not correctly managed when connecting with DFU.
123913 [CLI] It is not possible to write the LOCK byte.
123923 [UART] A timeout error occurs while disabling the readout protection.
124081 Odd behavior in the log when connecting a NUCLEO-F030R8 using the GUI.
124446 Request to add documentation for the getAuthID command.
124763 [OB] Wrong description of nBOOT1.
125039 [DFU] Strange behavior when trying to program in single-bank mode.
127099 [STM32L4+] Fail to program STM32L4+ twice in a row.
127311 The tool closes automatically when trying to load a file the path of which contains Chinese characters.
127978 Typo in option bytes: IWGDSTDBY.