STM32CubeProgrammer 2.13.0 released
STM32CubeProgrammer v2.13.0 release information
New features
- Added support for the STM32H5 series:
- STM32H563/573
- Debug authentication with password or certificate
- Authentication key provisioning
- Key generation
- Firmware encryption and signing
- Certificate generation
- STM32H503
- Debug authentication with password or certificate
- Firmware encryption and signing
- STM32H563/573
- Added support for the STM32WBA series:
- Flash memory and OTP programming, and option bytes
- Updated support for the STM32U5 series:
- STM32U535/545:
- SFI support (user interface and command-line interface) Flash memory, option bytes, RDP regression with password, and OTP programming.
- STM32U595/5A5:
- SFI update (user interface and command-line interface)
- SFIx update
- Via debug: user interface and command-line interface
- Via bootloader: command-line interface only
- STM32U535/545:
- Added support for the STLINK-V3PWR:
- Debug
- Bridge to bootloader interfaces (SPI, I2C, and CAN)
- Added new calculator features:
- Number converter
- File and flash memory checksum
Fixed issues
65657 Add the checksum display as done for the ST-LINK utility.
115829 [TrustedPackageCreator] Register naming mismatch between reference manual and .csv file.
116552 Possible attack on OEM1KEY and OEM2KEY.
129709 External flash memory programming issues in auto mode.
132975 [STM32G0] Erase selected sectors does not work properly on 256-Kbyte devices.
135017 [STM32CubeProg-GUI] Message must be updated while disabling RDP regression with password value.
135436 [API] Unhandled exception in writeMemory().
136195 [STM32CubeProg][STM32C0] STM32C031C4T6: wrong flash memory size.
136233 [CLI] ST-LINK serial number is ignored in shared mode.
137687 [CLI] Missing data from hex file when using safelib.
138051 [STM32CubeProg] STM32L5 CLI displaying protected flash memory content.
140627 [STM32CubeProg][STM32G4 256 Kbytes][0x495] Erase selected sectors does not work properly on 256-Kbyte devices with dual-bank mode (reopen).
140973 [STM32CubeProg-Connection] Connection issues for STM32G031J4M6.
141725 [STM32CubeProg][STM32G0 0x466] User configuration option bytes programming failed.
142009 [[STM32CubeProg-Register_Viewer] NVIC_ISERx[1-4] addresses are incorrect in the register viewer.
142286 [STM32H5][STM32CubeProg] Cannot erase the flash memory when TZEN=0.
Known problems and limitations
Download
https://www.st.com/en/development-tools/stm32cubeprog.html
Support
https://community.st.com/s/topic/0TO0X000000BX4uWAG/stm32cubeprogrammer