Skip to main content
Associate
April 8, 2024
Question

STM32CubeProgrammer 2.16.0 crashing in SWV

  • April 8, 2024
  • 0 replies
  • 687 views

Hello,

I'm using STM32CubeProgrammer version 2.16.0. The debugging works fine, but if the connection with the target is lost or probably some bad message is received on the client side, the application crashes. So in the first place I can't even see the last SWO messages that were received from the target.

Hardware: STM32U585 - SWD - HW Reset - ST-Link V2.0 ISOL @ V2J43S7

System log attached.

 

thx,

- Martin

This topic has been closed for replies.