Skip to main content

1 reply

Aziz BRIGUI
Technical Moderator
November 29, 2024

Hello @remov-b4-flight,

To provide more details on 171192. It comes from the non compatibility of the system bootloader with "Intel(R) USB 3.1 eXtensible Host Controller - 1.20 (Microsoft)"

=> Issue isn't a bug in the tool itself. With that being said, you have the following workarounds available:

1- Using a hub between PC and target

2- Rolling back to "Intel(R) USB 3.1 eXtensible Host Controller - 1.10 (Microsoft)"

3- Developing your own custom bootloader

STM32CubeProgrammer team is actively working on implementing a workaround to the issue inside the tool (Even though the issue isn't coming from the tool). I will keep you posted if I have any news

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.