STM32CubeProgrammer 2.4.0 Doesn't Open on Mac OS 10.10.5. "CubeProgrammer_API or one of its dependencies is missing"
Problem running STM32CubeProgrammer Version 2.4.0 on Mac OS Version 10.10.5.
Keeps throwing error "CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program or check your java architecture"
java -version returns
java version "1.8.0_251"
Java(TM) SE Runtime Environment (build 1.8.0_251-b08)
Java HotSpot(TM) 64-Bit Server VM (build 25.251-b08, mixed mode)
Please help. Thanks in advance.