STM32CubeProgrammer 2.6.0 released
New features
• Added the support for dual-core microcontrollers in the STM32WL Series
• Extended the support for the STM32G0 Series to the new STM32G0Bxxx and STM32G0Cxxx microcontrollers
• Added SFI support via JTAG/UART/SPI for STM32WL5xxx microcontrollers
• Added SFI support via I2C/SPI for STM32L5 Series microcontrollers
• Added SFIx support via bootloader for STM32L5 Series microcontrollers
• Added Sigfox™ credential provisioning support for STM32WL5xxx microcontrollers
• Added multiple Flash loader support for STM32 microcontrollers
• Added the SWV feature update (color support)
• Added the support for the server client HSM feature
• Added DFU IAP using custom PID/VID support for all STM32 products
• Added installer JRE bundle (OpenJDK)
Fixed issues
57835 Connect under reset with hardware reset is not working with SensorTile in low-power mode.
58716 Error when trying to mass erase STM32L0 128-Kbyte devices from CLI.
62639 RDP regression is not functional via BootLoader interfaces for STM32F030R8.
64267 Issues with FUS via USART boot mode.
70556 [STM32CubeProgrammer] Bug with STM32F765IGT6 (1-Mbyte Flash memory).
76987 [STM32CubeProg-STM32L5] STM32Cubeprog crash when communicating with the DFU app.
80586 [STM32CubeProg-STM32L0][CLI] Verification progress bar ends at 24%.
81647 User DFU functionality with STM32CubeProgrammer.
85313 [STM32CubeProg-STM32G0][GUI] Remove the BOR level section.
85898 Option Byte IRHEN must be deleted from STM32CubeProgrammer.
85960 STM32G431: STM32CubeProgrammer automatic mode download issue.
86576 [PRG] Fail to write OTP with STM32G4.
90060 [STM32CubeProgrammer][STM32L4] STM32L496: cannot connect using DFU IAP.
91608 Programming issue using the NUCLEO-L053R8 board connected via USB.
92038 STM32CubeProgrammer fails to open on macOS ® Catalina v 10.15.6.
92280 [STM32CubeProg-STM32H7][GUI] Erasing &Programming panel hangs (white panel).
92477 [STM32CubeProg-STM32L1][GUI] Incorrect memory size displayed and cannot make the erase.
92641 [STM32CubeProgrammer-Option Bytes] Cannot set STM32H743 IO_HSLV, VDDIO_HSLV option bit.
92674 [STM32CubePrg][STM32L0][DIE417] Cannot connect to board under reset when low power mode is activated.
92828 Seems no compatible OpenJFX version for Ubuntu ® 20.04 for OpenSTLinux.
93013 [CubePRG] CubeProgrammer_API.h not up to date in last STM32CubeProgrammer: missing 100 bytes in debugConnectParameters struct
93887 [CubePRG][0x451] Not possible to program STM32F765xG (Flash 1 Mbyte) using STM32CubeProgrammer v2.5.0.
93987 [STM32CubeProg-STM32G0][GUI] Remove NRST_MODE.
94517 [CubePRG] Cannot write 8 bytes in Flash memory using -w64 STM32CubeProgrammer CLI command.
Known problems and limitations
• STM32MP1 mircoprocessor get certificate operation is not complete in the UART mode.
• Production programming issues occur when using multiple ST-LINK in parallel.
• Installer: Insignificant message is returned during the installation when other instances are already installed.
• On some macOS ® machines, the STM32Cubeprogrammer GUI fails to launch (must be launched in CLI mode).
• The SFI operation via UART is not achieved and returns an error on macOS ® machines.
• STM32WB55: When trying to upgrade more than one stack, the operation can be done only with a second try.
• SFIx operation for STM32L5: An exception appears while programming when the –elbl command is not the first one in the command line.
Link