Skip to main content
RConf.1
Associate
May 13, 2021
Solved

STM32CubeProgrammer cannot connect to NUCLEO-F207ZG board in bootloader mode via UART interface

  • May 13, 2021
  • 1 reply
  • 1188 views

I have a NUCLEO-F207ZG board and STM32CubeProgrammer v2.7.0. I would like to use the embedded bootloader located in system memory.

So, first I activate bootloader mode pulling-up pin 138 (boot0) of the MCU. Then, in order to verify this first operation, I connect NUCLEO-F207ZG board to STM32CubeProgrammer via ST-LINK/V2-1 interface. The board connect succesfully and if I browse in the MCU Core menu I can see the Program Counter value is in the system memory range address.

My next step is to disconnect NUCLEO-F207ZG board from the STM32CubeProgrammer and to select the UART interface (configuration is shown in the attached image) . When I click the Connect button, I get the following message error (see also the attached image):

Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

I tried resetting the board, but it didn't solve the problem.

Could you tell me please how to solve this problem, please?

Thank you.

Best regards,

Riccardo

This topic has been closed for replies.
Best answer by Houda GHABRI

Hi @RConf.1​ ,

To connect this NUCLEO-F207ZG board in bootloader mode via UART interface you need to :

-Make sure that Boot0 is connected to VDD and Boot1 is connected to GND

-Make sure to connect RX/TX pin , you can use PB10 (USART3 in transmission mod) and PB11 pin(USART3 in reception mode )

-Select the appropriate port

0693W00000APADeQAP.png 

You can refer to AN2606 document for UART connection and Board schematic for pins .

If your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Houda

1 reply

Houda GHABRI
Houda GHABRIBest answer
ST Employee
May 21, 2021

Hi @RConf.1​ ,

To connect this NUCLEO-F207ZG board in bootloader mode via UART interface you need to :

-Make sure that Boot0 is connected to VDD and Boot1 is connected to GND

-Make sure to connect RX/TX pin , you can use PB10 (USART3 in transmission mod) and PB11 pin(USART3 in reception mode )

-Select the appropriate port

0693W00000APADeQAP.png 

You can refer to AN2606 document for UART connection and Board schematic for pins .

If your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Houda