[STM32CubeProgrammer][Fixed in 2.2.0]Add support for selecting all sectors
Dear STM32CubeProgrammer Developers,
I would recommend to add a select all checkbox/context menu to the page selector of the Erase flash memory table view:
I have a 2 sector wide EEPROM emulated area at the end of the flash what I would like to preserve during the erase operation, and to do so I need click all the 30 items. If a select all feature would be implemented I would only need to select all and untick the last two.
Thanks in advance!