Skip to main content
Associate
April 16, 2026
Question

STM32CubeProgrammer for macOS

  • April 16, 2026
  • 0 replies
  • 85 views

It would be nice if the further versions could be running on case sensitive file system on macOS.
Currently I need to use an USB key formatted APFS only. Then i can run the installer and install the programmer on this USB stick. As I most of the time only need the command line tools (*CLI) I copied the binaries and some folders with data on my case sensitive disk. They work fine. Only the GUI is not possible on the case-sensitive file system.