Skip to main content
PNenn.1
Visitor II
February 1, 2020
Question

STM32CubeProgrammer gives me an error

  • February 1, 2020
  • 1 reply
  • 594 views

I'm trying to program STM32L031 microcontroller using STLINK but STM32CubeProgrammer gives me the following error:

Error: No STM32 target found!

These are the conditions:

1) The hardware is correctly connected because the STM32CubeIde emulates correctly the target

2) I have updated the STLINK firmware to the last firmware release

3) I have tested the programmer on another computer and I get the same error

4) I already tested to power cycle several times the target and the emulator but nothing changes

Can someone help me?

Thanks in advance

Paolo

This topic has been closed for replies.

1 reply

Nesrine.JLASSI
Visitor II
October 30, 2020

Hi @PNenn.1​ 

Please try with the last STM32CubeProgrammer then tell me if it solve the issue.

Best regards,

Nesrine