STM32CubeProgrammer / STM32CubeIDE failed to connect STM32L476G-DISCO Board
Hello I am having a problem connecting my STM32L476G-DISCO Board using the STM32CubeProgrammer. When I received my board, I did managed to connect and download the compiled demo code, STM32CubeDemo_STM32L476G-Discovery-V1.0.5.hex successfully. The board is working fine as it shows the correct function on the display such as IDD, VDD, Record... the joystick works fine. But, I now wanted to change the code and debug it with my new code. So, I wrote some code and run the debugging in IDE, it could not connect the board anymore. So, I tried with STM32CubeProgrammer again to connect the board but, everytime when I click the connect button, it shows the message "Error: No STM32 target found!".
Can you please help me with this?
I can see the STMicroelectronics STLink Virtual COM Port in Device Manager.