STM32CubeProgrammer won't start up
Hi, I've just installed v2.14.0 for the first time, but it will not start up. All I get is the blue STM screen for a few second, then it disappears. I tried the command prompt start up detailed in This Post but I end up with an error message, shown below. I need help on how to proceed as I do not have JRE installed on my PC, but have had it in the past. I've tried re-installing STM32... but that didn't help
Exception in Application start method
java.lang.reflect.InvocationTargetException
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at com.sun.javafx.application.LauncherImpl.launchApplicationWithArgs(LauncherImpl.java:382)
at com.sun.javafx.application.LauncherImpl.launchApplication(LauncherImpl.java:321)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at sun.launcher.LauncherHelper$FXHelper.main(LauncherHelper.java:767)
Caused by: java.lang.RuntimeException: Exception in Application start method
at com.sun.javafx.application.LauncherImpl.launchApplication1(LauncherImpl.java:823)
at com.sun.javafx.application.LauncherImpl.lambda$launchApplication$1(LauncherImpl.java:181)
at java.lang.Thread.run(Thread.java:748)
Caused by: java.lang.Error:
There is an incompatible JNA native library installed on this system
Expected: 5.2.2
Found: 5.1.0
c:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\jre\bin;C:\WINDOWS\Sun\Java\bin;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\Common Files\Adobe\AGL;C:\Program Files (x86)\Brackets\command;C:\Program Files (x86)\nodejs\;C:\Ruby22\bin;C:\Users\stuar\AppData\Local\Programs\Python\Python36-32\Scripts;C:\Users\stuar\AppData\Local\Programs\Python\Python36-32;C:\Program Files\FileBot\;C:\WINDOWS\System32\OpenSSH\;C:\Program Files\PuTTY\;C:\Ruby22\bin;C:\Users\stuar\AppData\Local\Microsoft\WindowsApps;C:\Users\stuar\AppData\Roaming\npm;C:\Users\stuar\AppData\Local\atom\bin;%USERPROFILE%\AppData\Local\Microsoft\WindowsApps;;..
To resolve this issue you may do one of the following:
- remove or uninstall the offending library
- set the system property jna.nosys=true
- set jna.boot.library.path to include the path to the version of the
jnidispatch library included with the JNA jar file you are using