Skip to main content
Associate
December 12, 2024
Question

STM32F4 fails to verify after programming with STM32_Programmer_CLI over USB

  • December 12, 2024
  • 1 reply
  • 689 views

I have manually verified the FLASH bytes are correct after programming, but the -v option results in "Error: Data mismatch found at address 0x10000000 (byte = 0x21 instead of 0x00)" and the process stops.

Isn't 0x10000000 a CCM address and why is it being tested and failing?  See terminal output below:

 

"C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=USB1 -d "fw.hex" -v -g 0x08000000
-------------------------------------------------------------------
STM32CubeProgrammer v2.18.0
-------------------------------------------------------------------

 

USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode
SN : 000000
DFU protocol: 1.1
Board : --
IAP
Opening and parsing file: fw.hex


Memory Programming ...
File : fw.hex
Size : 459.21 KB
Address : 0x080A0000


Erasing memory corresponding to segment 0:
Erasing memory corresponding to segment 1:
Download in Progress:
██████████████████████████████████████████████████ 100%██████████████████████████████████████

File download complete
Time elapsed during download operation: 00:00:28.989

 

Verifying ...


Read progress:
██████████████████████████████████████████████████ 100%

Error: Data mismatch found at address 0x10000000 (byte = 0x21 instead of 0x00)


Error: Download verification failed

 

1 reply

scottroAuthor
Associate
December 12, 2024

Tracked the issue down to the HEX file including bytes to initialize CCM memory as "segment 1".

The ST code must be using CCM for scratch space...

 

Resolved.