STM32F411CEU6: ST LINK DEBUGGER not working properly
Hi Team,
When I tried to flash the code to stm32f411ceu6 using the stlinkv2, I was getting the error "Error in initializing ST-LINK device.
Reason: No device found on target.
This error was corrected using the STM32 ST-Link UTILITY. When the USB cable is first plugged in, hold down the reset button, and immediately select Target->Erase Chip upon release. Once the chip is erased, the bootloader will be able to utilize the USB connection correctly and you will be able to use the USB port to program.
After this, I did a Mass Erase (Full chip erase)in the STM32CubeProgrammer. STLINK got connected in STM32CubeProgrammer. But while flashing the code to the STM32 MCU, We are getting the error:"Target not responding, retrying".
Kindly provide a solution. Waiting for reply
Thanks and Regards
Anitta Darwin