STM32G0 External Loader for I2C eeprom
Hi,
I try to make a external loader for STM32G030.
I was implemented function MassErase(), Write(), Read(), Init()...
First I test function on "flash" version and everything work. But when I try using it in STM32CubeProgrammer the Write function not working.
Full chip erase work ok, and after this operation eeprom is cleared by 0xFF as default data.
But when I try write to eeprom, it stuck on "Loader write range..."
Both function (MassErase and Write) use this same function to write data to eeprom.
What could be the reason that cube stop in this?
13:58:17:879 : Memory Programming ...
13:58:17:879 : Opening and parsing file: test13.hex
13:58:17:880 : File : test13.hex
13:58:17:881 : Size : 128.00 B
13:58:17:882 : Address : 0x00000000
13:58:17:882 : Erasing Segment <0> Address <0x00000000> Size <128>Bytes
13:58:17:882 : Erasing memory corresponding to segment 0:
13:58:17:883 : Memory erase...
13:58:17:883 : halt ap 0
13:58:17:883 : w ap 0 reg 15 PC (0x20000000)
13:58:17:883 : w ap 0 reg 17 MSP (0x20000500)
13:58:17:883 : w ap 0 reg 16 xPSR (0x01000000)
13:58:17:883 : w ap 0 @0x20001C40 0x00000200 bytes Data 0x00000000
13:58:17:892 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
13:58:17:906 : w ap 0 @0x20000004 0x00001804 bytes Data 0x00000000
13:58:17:906 : Erasing external memory sectors [0 7]
13:58:17:906 : Init flashloader...
13:58:17:907 : halt ap 0
13:58:17:907 : w ap 0 reg 0 R0 0x00000001
13:58:17:907 : w ap 0 reg 1 R1 0x00000000
13:58:17:907 : w ap 0 reg 2 R2 0x00000000
13:58:17:907 : w ap 0 reg 3 R3 0x00000000
13:58:17:907 : w ap 0 reg 4 R4 0x00000000
13:58:17:907 : w ap 0 reg 5 R5 0x00000000
13:58:17:908 : w ap 0 reg 6 R6 0x00000000
13:58:17:908 : w ap 0 reg 7 R7 0x00000000
13:58:17:908 : w ap 0 reg 8 R8 0x00000000
13:58:17:908 : w ap 0 reg 9 R9 0x00000000
13:58:17:909 : w ap 0 reg 10 R10 0x00000000
13:58:17:909 : w ap 0 reg 11 R11 0x00000000
13:58:17:909 : w ap 0 reg 12 R12 0x00000000
13:58:17:909 : w ap 0 reg 13 SP 0x00000000
13:58:17:909 : w ap 0 reg 14 LR 0x20000001
13:58:17:916 : w ap 0 reg 15 PC 0x2000071D
13:58:17:918 : w ap 0 reg 16 xPSR 0x01000000
13:58:17:920 : w ap 0 reg 17 MSP 0x20001C04
13:58:17:920 : w ap 0 reg 18 PSP 0x00000000
13:58:17:920 : run ap 0
13:58:17:920 : halt ap 0
13:58:17:921 : r ap 0 reg 0 R0 0x00000001
13:58:17:921 : Loader sector erase...
13:58:17:921 : w ap 0 reg 0 R0 0x00000000
13:58:17:921 : w ap 0 reg 1 R1 0x00000070
13:58:17:921 : w ap 0 reg 2 R2 0x00000002
13:58:17:921 : w ap 0 reg 3 R3 0x00000000
13:58:17:921 : w ap 0 reg 4 R4 0x00000000
13:58:17:921 : w ap 0 reg 5 R5 0x00000000
13:58:17:921 : w ap 0 reg 6 R6 0x00000000
13:58:17:922 : w ap 0 reg 7 R7 0x00000000
13:58:17:922 : w ap 0 reg 8 R8 0x00000000
13:58:17:922 : w ap 0 reg 9 R9 0x00000000
13:58:17:922 : w ap 0 reg 10 R10 0x00000000
13:58:17:922 : w ap 0 reg 11 R11 0x00000000
13:58:17:922 : w ap 0 reg 12 R12 0x00000000
13:58:17:922 : w ap 0 reg 13 SP 0x00000000
13:58:17:922 : w ap 0 reg 14 LR 0x20000001
13:58:17:924 : w ap 0 reg 15 PC 0x20000791
13:58:17:924 : w ap 0 reg 16 xPSR 0x01000000
13:58:17:925 : w ap 0 reg 17 MSP 0x20001C04
13:58:17:926 : w ap 0 reg 18 PSP 0x00000000
13:58:17:927 : run ap 0
13:58:18:082 : halt ap 0
13:58:18:083 : r ap 0 reg 0 R0 0x00000001
13:58:18:083 : erase: 0205ms
13:58:18:083 : Download in Progress:
13:58:18:087 : Size : 128 Bytes
13:58:18:087 : Address : 0x00000000
13:58:18:087 : Buffer program...
13:58:18:087 : halt ap 0
13:58:18:087 : w ap 0 reg 15 PC (0x20000000)
13:58:18:088 : w ap 0 reg 17 MSP (0x20000500)
13:58:18:088 : w ap 0 reg 16 xPSR (0x01000000)
13:58:18:088 : w ap 0 @0x20001C40 0x00000200 bytes Data 0x00000000
13:58:18:088 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00
13:58:18:127 : w ap 0 @0x20000004 0x00001804 bytes Data 0x00000000
13:58:18:127 : Loader write range...