Skip to main content
mcelik
Associate
December 6, 2023
Question

STM32g474 processor nSWBOOT0 default option byte

  • December 6, 2023
  • 1 reply
  • 1368 views

We want to update the software of STM32G474 processor via uart. However, when we look at the "Pattern 14" option in the bootloader settings for this processor, the "nSWBOOT0" option byte is requested to be 1. However, we see that the default setting is "0" (Unchecked). Changing this option byte from the cubeprogrammer programme in mass production will be a great difficulty for us. Is there another easy method for this?

This topic has been closed for replies.

1 reply

STTwo-32
Technical Moderator
December 6, 2023

Hello @mcelik and welcome to the ST Community :).

I suggest you contact your local sales and marketing office or create an ols support ticket. Also, you should give the datecode and the marking of the chip.

Best Regards.

STTwo-32.