STM32H562RIT6 is not programmed
Hi
I have designed a header board for the STM32H562RIT6 microcontroller, but no matter how hard I try, I can't program it! The wiring is as follows. Please guide me on how to program this microcontroller. If there are any tips or specific instructions for programming this microcontroller, I would appreciate your help.
WIRING ( SIMILAR TO AN5711 PAGE 36 ) :
All VDD and VDDA pins → connect to 3.3V
All VSS and VSSA pins → connect to GND
BOOT0 → connect to GND through a 10kΩ resistor
RESET → connect to GND through a 100nF capacitor
Connect the two VCAP pins together, and connect each pin to a 2.2µF capacitor
PROGRAMMER : ST-LINK V2 ( 3.3V , GND , SWDIO , SWCLK )