STM32H753I-Eval2 in DFU mode
Hello,
I'm curious if I am going through the correct procedure to put th H753I eval board in DFU mode. I have the power jumper JP10 on PSU. I then put a jumper on JP3 which is labeled BL_BOOT0 (which as far as I know puts the H7 in DFU mode when pulled high). I then plug in the PSU and then plug in usb cable to my pc and to the eval board. I've tried all three OTG ports, but I get no activity on my pc. When I check device manager, nothing new shows up at all. I've seen other see STM32 BOOTLOADER and STM32 in DFU mode, but I don't see either of these.
Any help or insight would be appreciated. Thank you.