Associate
May 2, 2022
Question
STM32L152VD-X reserved memory space
- May 2, 2022
- 4 replies
- 1764 views
Hello,
I am using the STM32CubeProgrammer, version 2.10.0, and it does not detect the STM32L152VD-X reserved memory space, at address 0x0803000.
The STM32CubeProgrammer detects the correct device ID which is 0x437 but does not detect the correct device.
If I open the STM32_Prog_DB_0x437.xml file I see that the STM32L152VD-X is not even implemented.
This allows me to write to this reserved memory space which I believe is not a good idea
Questions:
- Is the STM32L152VD-X implemented in the STM32CubeProgrammer?
- What is the impact of writing to the reserved memory space?