Skip to main content
AM-adben
Associate II
January 3, 2025
Solved

STM32N6570-DK: Unable to erase external flash

  • January 3, 2025
  • 1 reply
  • 2203 views

Hi, I can't erase the external flash or write a new binary on my STM32N6570-DK board. My problem is similar to this post: STM32N6570-DK: Cannot erase external Flash. But the solution in that post didn't work for me.

I have tried using two external loaders (MX66UW1G45G, OTP_FUSES) and also with only one loader (MX66UW1G45G). But everytime the erase is failed with this message: `Error: Mass erase operation failed. Please verify flash protection`.

I am sharing some screenshots and my OTP export for your reference.

Please let me know how to unlock the flash so I can program it.

OTP screenshotOTP screenshot2 loaders are selected here. But I tried with only one loader too.2 loaders are selected here. But I tried with only one loader too.

Best answer by AM-adben

Thank you. Setting the boot mode to "Development Boot" fixed the problem and now it's possible to write to the external flash. For STM32N6570-DK, the Dev_boot mode is set when BOOT1 switch position is 1-3, BOOT0 switch position doesn't matter.

As mentioned in the answer you shared:


The Dev_Boot has been designed to open the STM32N6 debug port to external tools for debugging applications and programming/erasing internal or external memory and also to fuse OTP bits (see RM0486 section 5 OTP mapping).

Thank you for your quick assistance.

1 reply

Amel NASRI
Technical Moderator
January 3, 2025

Hi @AM-adben,

The answer from @RomainR. in NUCLEO-N657X0-Q: failed to start GDB server can give you some hints.

For STM32N6570-DK documentation, please refer to https://www.st.com/en/evaluation-tools/stm32n6570-dk.html.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AM-adben
AM-adbenAuthorBest answer
Associate II
January 3, 2025

Thank you. Setting the boot mode to "Development Boot" fixed the problem and now it's possible to write to the external flash. For STM32N6570-DK, the Dev_boot mode is set when BOOT1 switch position is 1-3, BOOT0 switch position doesn't matter.

As mentioned in the answer you shared:


The Dev_Boot has been designed to open the STM32N6 debug port to external tools for debugging applications and programming/erasing internal or external memory and also to fuse OTP bits (see RM0486 section 5 OTP mapping).

Thank you for your quick assistance.