Skip to main content
CAben.1
Associate II
January 17, 2022
Question

Target is not responding, retrying... (Nucleo L073RZ board)

  • January 17, 2022
  • 2 replies
  • 1583 views

Hello Everyone,

II'm currently working with my Nucleo L073RZ board and so far my program built successfully but i cant upload it. Nonetheless, other programs are still able to run well on the board. I dont understand what i am doing wrong. I have read other responses to similar questions but i still cant find a solution. Please I will be glad to get some help/ideas on how to solve this. Thank you.

Best Regards!

STMicroelectronics ST-LINK GDB server. Version 6.0.0

Copyright (c) 2021, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.9.0-RC01          

   -------------------------------------------------------------------

ST-LINK SN : 066BFF495257808667041449

ST-LINK FW : V2J39M27

Board    : NUCLEO-L073RZ

Voltage   : 3.26V

SWD freq  : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x447

Revision ID : Rev Z

Device name : STM32L07x/L08x/L010

Flash size : 192 KBytes

Device type : MCU

Device CPU : Cortex-M0+

BL Version : --

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a03832.srec

 File     : ST-LINK_GDB_server_a03832.srec

 Size     : 31856 Bytes

 Address    : 0x08000000 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 248]

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:02.973

Verifying ...

Download verified successfully 

Shutting down...

Target is not responding, retrying...

This topic has been closed for replies.

2 replies

Technical Moderator
January 19, 2022

Hello @CAben.1​ ,

Maybe you should check the SWD connector.

Did you try ST-Link Utility to solve this problem?

Try with the ST-Link Utility and "connect under reset" mode, then "full chip erase" option.

I'll be waiting for your feedback.

Imen

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Visitor II
May 6, 2024

Hi i have the same issue and I tried st link utility and did not work.

Tesla DeLorean
Guru
May 6, 2024

You likely have a SIMILAR issue.

Perhaps looks at what you did to the target IC to block debug access, say disabled SWD/JTAD operation, reconfigured the pins the debugger uses (PA13, PA14, PB3, etc), or that you powered-off the circuitry that needs to be running for this to work. ie put the device in Low Power / Standby modes?

Pull BOOT0 pin HIGH so YOUR CODE doesn't run and break access.

The ST-LINK Utilities have been deprecated for many years, migration to STM32 Cube Programmer is STRONGLY recommended.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
Visitor II
May 6, 2024

i tried stm32 cube programmer too. now to don't get the error "Target is not responding, retrying..." . I get "Download verified successfully". but when I resume the code its not running