UART Bootloader connection via API
Hi everyone,
this is my first post, as I have always been able to solve my problems thanks to your help. Unfortunately, I can't find a solution regarding the CubeProgrammer API, which I am currently working on.
I am developing an update tool that will use the internal bootloader of a STM32H743. For this, I am developing a C++ programm, using Visual Studio 2026 Version 18.2.0 with .Net Framework Version: 4.8.09221. CubeProgrammer_API.h and all neccessary .dll files are included as described in the documentation. There are no compiler errors or warnings.
I used the attached UART example for testing but it is not possible to connect to my device. COM ports are detected by getUsartList function as expected. If I try to connect with function connectUsartBootloader as shown in the example I will get error -5 ( CUBEPROGRAMMER_ERROR_NOT_SUPPORTED ). Nevertheless, it is possible to establish a connection and execute a file upload with STMCubeProgrammer GUI and also with STMCubeProgrammer CLI via a serial port.
I checked already communication with a logic analyzer. Everything looks good, commands and responses are the same (STMCubeProgrammer GUI and custom tool) as shown in picutre below . Commands from custom tool are marked in red and device response is marked in orange.

After this communication sequence connectUsartBootloader function is aborted and error -5 occurs. No clue why this happens. It looks like the API does not support used MCU. Anyway it works with GUI and CLI so it also should work with the used API.
Does anyone have an idea how to solve this problem?