UART PROGRAMM ERROR ON STM32F407 WITH STM32CUBPROGRAMMER V2.2.0
Dear all,
I want to program my STM32F407 by UART.
I can connect to the microcontroller correctly by uart. boot0 is high and boot1 is low.
I can read the pre-programmed code by the uart.
I can erase the microcontroller.
But I cannot program my stm32f407. The error is :
"Error: Write Command not acknowledged at address 0x8000000"
"Error: failed to download Segment[0]"
"Error: failed to download the File"
I can program my stm32f407 by STMFlashLoader very well. But i want to program by stm32cube programmer.
Please help me.
Thanks alot.