Question
Ubuntu 25.10 - STM32CubeProgrammer upgrade fail.
- December 15, 2025
- 1 reply
- 557 views
Launched STM32CubeProgrammer v2.20.0 after a long time since last use - it prompts an update available via an icon button.
Clicked the icon, clicked Next, ticked a box, clicked "install Now", it starts download ing a big file...
When the file has finished downloading it then displays an error message - see attached screenshot.
Unable to unzip file: /home.main/.STM32CubeProgrammer/downloads//STM32CubeProgrammer2.21.0_linux64.zip
Note the double slash // in the path.
Also tried launching it direct from a terminal prompt out of my /opt folder.... same result.