Unable to Programm Blue pill
When I try to program my Blue Pill over UART in the Stm32CubeProgrammer it give me this Error message:
13:11:23 : Serial Port ttyUSB0 is successfully opened.
13:11:23 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1,0, flow-control = off
13:11:23 : Activating device: OK
13:11:23 : Board : --
13:11:23 : Chip ID: 0x410
13:11:23 : BootLoader protocol version: 3.0
13:11:23 : UPLOADING OPTION BYTES DATA ...
13:11:23 : Bank : 0x00
13:11:23 : Address : 0x1ffff800
13:11:23 : Size : 16 Bytes
13:11:23 : UPLOADING ...
13:11:23 : Size : 1024 Bytes
13:11:23 : Address : 0x8000000
13:11:23 : Read progress:
13:11:23 : Data read successfully
13:11:23 : Time elapsed during the read operation is: 00:00:00.106
13:11:54 : Memory Programming ...
13:11:54 : Opening and parsing file: blinky-test-f1-1.5.hex
13:11:54 : File : blinky-test-f1-1.5.hex
13:11:54 : Size : 12,47 KB
13:11:54 : Address : 0x08000000
13:11:54 : Erasing memory corresponding to segment 0:
13:11:54 : Erasing internal memory sectors [0 7]
13:11:54 : Erasing memory corresponding to segment 1:
13:11:54 : Erasing internal memory sectors [8 12]
13:11:54 : Download in Progress:
13:11:55 : File download complete
13:11:55 : Time elapsed during download operation: 00:00:01.549
13:11:55 : Verifying ...
13:11:55 : Read progress:
13:11:57 : Download verified successfully
13:11:57 : RUNNING Program ...
13:11:57 : Address: : 0x08000000
13:11:57 : Start operation achieved successfully
13:11:57 : Error: GETID command not acknowledged!
13:11:57 : Reemission of GetID command
13:11:57 : Error: GETID command not acknowledged!
13:11:57 : Reemission of GetID command
13:11:58 : Timeout error occured while waiting for acknowledgement.
13:11:58 : Error: GETID command not acknowledged!
13:11:59 : Timeout error occured while waiting for acknowledgement.
13:11:59 : Error: GETID command not acknowledged!
13:11:59 : Reemission of GetID command
13:12:00 : Timeout error occured while waiting for acknowledgement.
13:12:00 : Error: GETID command not acknowledged!
13:12:00 : Reemission of GetID command
13:12:01 : Timeout error occured while waiting for acknowledgement.
13:12:01 : Error: GETID command not acknowledged!
13:12:02 : Timeout error occured while waiting for acknowledgement.
13:12:02 : Error: GETID command not acknowledged!
13:12:02 : Reemission of GetID command
13:12:03 : Timeout error occured while waiting for acknowledgement.
13:12:03 : Error: GETID command not acknowledged!
13:12:03 : Reemission of GetID command
13:12:04 : Timeout error occured while waiting for acknowledgement.
13:12:04 : Error: GETID command not acknowledged!
13:12:05 : Warning: Connection to device 0x410 is lost
13:12:05 : Disconnected from device.
How do I fix this?