Skip to main content
Felix1
Associate
May 31, 2019
Question

Use STM32CubeProgrammer API will show Error: Device not supported

  • May 31, 2019
  • 0 replies
  • 543 views

Hi All

My customer try to use STM32CubeProgrammer API, when run the UART Bootloader Example will show "Error: Device not supported",

How to fixed this issue?

Hardware platform: NUCLEO-G070RB

STM32Cubeprogrammer API version: 2.1.0

As below is log file content.

STM32CubeProgrammer API v2.1.0

+++ UART Bootloader Example +++

------------- Serial Port List --------------

Port Name [0] : COM3

Port Name [1] : COM5

---------------------------------------------

Serial Port COM5 is successfully opened.

Port configuration: parity = even, baudrate = 115200, data-bit = 8,

           stop-bit = 1.0, flow-control = off

QObject::startTimer: Timers can only be used with threads started with QThread

Activating device: OK

Chip ID: 0x460

BootLoader protocol version: 3.1

Error: Device not supported

This topic has been closed for replies.