Skip to main content
Js.1
Associate
September 9, 2020
Question

Wont launch on Mac 10.15.6, binary improperly signed.

  • September 9, 2020
  • 0 replies
  • 547 views

First off I am running java 8:

java version "1.8.0_261"

Java(TM) SE Runtime Environment (build 1.8.0_261-b12)

Java HotSpot(TM) 64-Bit Server VM (build 25.261-b12, mixed mode)

Ive tried installing this software two different ways:

java -jar SetupSTM32CubeProgrammer-2.5.0.exe

and

java jar SetupSTM32CubeProgrammer-2.5.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-2_5_0_macos

Once I've installed it I've tried running three different ways

clicking the app

clicking the app within the package contents

java -jar /Applications/STMicroelectronics/STM32Cube/STM32CubeProgrammer/STM32CubeProgrammer.app/Contents/MacOs/bin/STM32CubeProgrammerSTM32CubeProgrammer

There's no STM32CubeProgrammer.exe like I've seen mentioned by support

all ways of opening the app cause the following error in console or through a pop up it offers to report:

com.apple.xpc.launchd[1] (com.st.stm32cubeprogrammer.8224[742]): Binary is improperly signed.

This topic has been closed for replies.