Zephyr images signed with STM32CubeProgrammer 2.21.0 do not run
Following the directions in https://docs.zephyrproject.org/latest/boards/st/stm32n6570_dk/doc/index.html images signed using STM32_SigningTool_CLI version 2.20.0 run OK on the board.
However, after upgrading to STM32CubeProgrammer 2.21.0, images no longer run (I believe the signature check is now failing on the device).
Reverting back to 2.20.0 fixes the signing issue on Windows, macOS, and Linux for the STM32N6570-DK board.
However, this is a blocker for developers using the Nucleo N657X0-Q board on Windows & Ubuntu because 2.20.0 has a bug which causes west flash to fail for this board on both Windows & Ubuntu. This west flash bug is fixed for Windows & Ubuntu in 2.21.0, but we can't use that version due to the signing issue in 2.21.0.