12v dc 4 channel relay module / Error : Cannot communicate with the device !
Hi everyone,
I have 12v dc 4 channel relay module which have stm8s103f3 on it.
i am using ST visual develop and STVP to flash program using ST-Link V2 programmer.
ST-Link V2 Pins: 1- RST, 3- GND, 5- Swim, 7- 3.3v (which is required for relay module).
when i make the connections as above pinouts and try to program using In ST programmer, the module gets turned ON but it gives:
Error : Cannot communicate with the device !
Check the SWIM cable connection and check all the needed pin connections on the SWIM connector.
If the application code uses Swim Disable and Reset pin as Output or has disabled SWIM Clock Divider:
Try Now to SWITCH OFF and ON the application Power Supply while NRST Reset pin is forced low.
Error : < PROGRAM MEMORY verifying failed.
I have attached the image of Module and programmer.
please help to find the solution on it.
Thanks, and regards.
Saurav.