Question
About STM8S Flash block write
The chip I use is STM8S003F3. When using Flash block erase, it is executed in RAM. If the offset of the Flash address is used with a 32-bit variable, the execution will cause an error. Can this 8-bit microcontroller use 32-bit addressing in RAM?