Question
Active/Halt wakeup with RTC
Posted on May 03, 2013 at 14:36
Hi ,
I am a new user of STM8. In my project I am using Active/halt mode an it wakes up with RTC Wakeup operation. My problem is, it is always waking up same times. it's equal to 3ms. I want update auto wake up times. I am trying to change RTC_SetWakeUpCounter(30000) but it is not setting wake up times. How can ı change wake up times.Thank you for your comments.Here is the example code;///////////////////////////////////////////////////////////////////#include ''stm8l15x.h''#include ''stm8l151f3.h''#define ENABLE 1#define DISABLE 0void RTC_Config(void){ RTC_WriteProtectionCmd(DISABLE); CLK_RTCClockConfig(CLK_RTCCLKSource_LSI, CLK_RTCCLKDiv_1); while (CLK_GetFlagStatus(CLK_FLAG_LSIRDY) == RESET); CLK_PeripheralClockConfig(CLK_Peripheral_RTC, ENABLE); RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div2); RTC_ITConfig(RTC_IT_WUT, ENABLE); enableInterrupts();}void GPIO_LowPower_Config(void){ GPIO_Init(GPIOA, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow); GPIO_Init(GPIOB, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_7, GPIO_Mode_Out_PP_Low_Slow); GPIO_Init(GPIOB, GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5, GPIO_Mode_Out_PP_High_Slow); GPIO_Init(GPIOC, GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6, GPIO_Mode_Out_PP_Low_Slow); GPIO_Init(GPIOD, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow); GPIO_Init(GPIOE, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow); GPIO_Init(GPIOF, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Slow);}void Halt_Init(void){ PWR_PVDCmd(DISABLE); /* Switch to LSI as system clock source */ /* system clock prescaler: 1*/ CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1); CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_LSI); CLK_SYSCLKSourceSwitchCmd(ENABLE); while (CLK_GetFlagStatus(CLK_FLAG_LSIRDY) == 0); CLK_HSICmd(DISABLE); CLK_HSEConfig(CLK_HSE_OFF); /* Set STM8 in low power */ PWR_UltraLowPowerCmd(ENABLE); /* Set GPIO in low power*/ GPIO_LowPower_Config(); /* Stop RTC Source clock */ RTC_WriteProtectionCmd(DISABLE); RTC_Config(); RTC_WriteProtectionCmd(DISABLE);CFG_GCR&=0xFD; RTC_SetWakeUpCounter(30000); RTC_WakeUpCmd(ENABLE); CLK_PeripheralClockConfig(CLK_Peripheral_LCD, DISABLE);}void main(void){ Halt_Init(); halt();while(1){//GPIO_ToggleBits(GPIOB,GPIO_Pin_0);}}/////////////////////////////////////////////////////////////