Skip to main content
Visitor II
June 7, 2018
Question

Advanced TIM1/TIM5 sync on STM8S903

  • June 7, 2018
  • 1 reply
  • 1072 views
Posted on June 07, 2018 at 21:07

I'm having a little confusion interpreting the STM8S reference and STM8S903 data sheet.  The STM8S903 is the part with TIM5 and TIM6 instead of TIM2 and TIM4, and adds the advanced triggering mechanism that allows linking the timers via trigger signals.

I'm feeding TIM1 an external clock via TIM1-ETR, and using all four CAPCOM output channels to drive external pins.  The advanced features of TIM1 work well for this, since it has those four external channel pins and the ability to use an external pin as the clock source.

There is also a comment in the STM8S reference (�17.4.5) that says, '

External clock mode 2 can be used with another trigger mode. For example, the ETR can be used as the external clock input, and a different input can be selected as trigger input (in trigger standard mode, trigger reset mode, or trigger gated mode).

'

I would like to

- use TIM1_ETR as TIM1's clock (external clock mode 2)

- also use TIM1_ETR pin to reset/restart TIM5 (trigger reset mode)

- use TIM5 TRGO to reset TIM1 (trigger reset mode)

- pause or freeze TIM5 when it resets TIM1, until it is reset by TIM1_ETR

FWIW, my design constraints prevent me from simply polling the TIM1 counter in the main loop (there are plenty of examples for that), and I'd like more accuracy on when TIM1 is reset than what I can get from polling within a timer-driven ISR.  Plus, I relish the challenge of learning the STM8S903 part and how its timers can be linked.

Is there anyone out there with experience on the STM8S903 that can confirm this configuration is possible and/or give hints on its implementation?

#trgo #trgo-itr3 #stm8s903 #tim5
    This topic has been closed for replies.

    1 reply

    Visitor II
    June 11, 2018
    Posted on June 11, 2018 at 11:30

    To answer my own question after some research, it doesn't look like it's possible on the STM8S903.

    Only TIM1 can use T1_ETR as an external clock ( TIM1_ETR[ECE] = 1 ).  Plus only TIM1 can use T1_ETR as a trigger source ( TIM1_SMCR[TS] = 111 ).

    The other timers on the STM8S903 that can be synced (TIM4 & TIM6) do not permit T1_ETR to be used as a trigger source.  Their only options are the ITRx lines fed from the other timers' TRGO signal.  Those are setup in TIMx_CR2[MMS] and are limited to the timer's reset, enable, and update events (plus various compare settings on TIM1).

    The docs say TIM5 shares the TIM1_ETR external trigger input (§18.3), but I have not found one place that is true. 

    :(