Skip to main content
Visitor II
June 18, 2018
Question

AN1447 SOFTWARE DRIVER FOR 4-MULTIPLEXED LCD WITH A STANDARD ST62

  • June 18, 2018
  • 1 reply
  • 1106 views
Posted on June 18, 2018 at 14:12

The ST62 is obsolete. Is there a direct hardware replacement processor that would work in this application? Would the supplied software program for the ST62 be compatible with the new processor?

Thanks

#multiplex-lcd
    This topic has been closed for replies.

    1 reply

    Graduate II
    June 18, 2018
    Posted on June 18, 2018 at 15:01

    Really not sure there is any support for these 20+ year old families.

    You should probably find a local ST rep or FAE and work with them to redesign/migrate the current use case, and understand your options.

    You would likely need to find the source for your existing program, and recreate with current tools. A lot of DOS stuff isn't going to work at all with 64-bit Windows platforms.

    An STM8 or STM32 (20-pin Cortex-M0) device should be able to driver available 7-segment displays

    http://www.st.com/content/ccc/resource/technical/document/application_note/28/3c/6b/8b/3c/b9/45/c0/CD00004279.pdf/files/CD00004279.pdf/jcr:content/translations/en.CD00004279.pdf