Skip to main content
Graduate II
March 30, 2023
Question

Any tips to solve this APPCRASH ntdll.dll error?

  • March 30, 2023
  • 1 reply
  • 937 views

Hello,

Problem opening the Programmer, I can't click on the Integrated Circuit icon.

The error occurs almost always, eventually when reinstalling, once or twice the programmer window opens correctly. After giving this error, it does not open again and only presents an error.

The problem occurs even in a newly installed system, 32 or 64 bits.

Tested with Windows 7 and Windows XP, which System should work?

Since 2017 there are no updates. Any possibility of making a plugin for Eclipse?

The SDCC compiler already supports STM8S, and it works on Linux as well.

0693W00000bhCskQAE.png

    This topic has been closed for replies.