Can I swap TX & RX USART1 STM8L152
Hi Everyone,
I have an issue with USART1 where my board designer mixed up the TX and RX pins going to an external module. Is there any way to swap them in software? I've had a look though the reference manual and seen the remapping feature but its not what I need and I know about the SWAP feature but it doesnt seem to be availble on my chip.
I'm fairly sure it's not possible without bitbanging but just checking to be sure.
Also If bitbanging is the only option, would it be possible to acheive at 115200? This is the default baud rate of the receiving module and I won't be able to change it until I can communicate with it.
Thanks,
Tiarnan