Question
Can't configure Timer2 configuration registers
Posted on August 13, 2012 at 16:15
Hi.
I'm trying to use Input Capture mode on Timer2 (channel 3) on an STM8S105 (discovery board). It won't work, and when i m watching peripheral registers with appropriated breakpoints, the registers aren't changing from default value. I m using STVD with cosmic compiler. I'm using firmware libraries. (i already checked out, that every macros was pointing to the right register.) Here's everything relevant in my code : CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER2, ENABLE); GPIO_Init(GPIOD, GPIO_PIN_2, GPIO_MODE_IN_PU_NO_IT);//!\ modify option bytes : select TIMR2-CH3 for AFR1
TM2_DISABLE; //macro resetting CEN bit in TMR2->CR1 register
TIM2_DeInit();
TIM2_TimeBaseInit(TIM2_PRESCALER_1, 0xFEFE); // changed from FFFF to FEFE to see if it applies any change to ARR register, and it does not :\
TIM2_ICInit(TIM2_CHANNEL_3,
TIM2_ICPOLARITY_FALLING,
TIM2_ICSELECTION_DIRECTTI,
TIM2_ICPSC_DIV1,
0);
TIM2_ITConfig(TIM2_IT_CC3, ENABLE);
TIM2_CCxCmd(TIM2_CHANNEL_3, ENABLE);
TM2_ENABLE; //macro setting CEN bit in TMR2->CR1 register Has anyone a clue on chat i forgot to enable so this peripheral might work ?