Question
Cannot compile with Cosmic
Posted on February 26, 2016 at 03:20
Hi,
I'm trying to use the Cosmic 32K compiler in ST Visual develop and having created a completely new project with no additional code in, I can't compile it. I can't compile using Idea either.My error is:&sharperror cpstm8 C:\Program Files (x86)\COSMIC\32K_Compilers\CXSTM8\Hstm8\mods0.h:1 FlexLM No such feature exists.main.c: The command: ''cxstm8 +debug -pxp -no -l +mods0 -pp -i''C:\Program Files (x86)\COSMIC\32K_Compilers\CXSTM8\Hstm8'' -clDebug\ -coDebug\ main.c '' has failed, the returned value is: 1exit code=1.Could anybody advise me on how to solve this?Thanks, #stvd-cosmic-compiler-stm8l