Cannot connect ST-Link
I am trying to program a hex file in STM8S103F2P6 using ST-Link via STVP
However, I get the error
> Programming PROGRAM MEMORY area...
Error : Cannot communicate with the board.
Wrong board selection or check board power supply or check that a previous session is closed.
Error : < PROGRAM MEMORY programming failed.
Configuration:
Windows SP3,
STLINK V1,
Firmware: V1.J12.S3 JTAG+SWIM Debugger
Target: STM8S103F2P6
Is there another utility that can be used to program STM8S via ST-Link.
Thanks.
#stlink #stm8-swim-connect