Could the STM8AL board of STMA-Discovery kit be debuged and connected to Peak Lin at the same time ?
Hello, I have a question about STMA-Discovery Boards.
I want to use just one board which is STM8AL one, without connecting it with STM8AF, and i want to make LIN communication using Peak Lin (which requires an exterior 12V power supply).
Normally to debug the stm8 board it is done through the USB power cable (5V) but if I want to debug and connect Peak LIN at the same time the board will be connected to 5V (from the debug cable) and to 12V (from the exterior power source) at the same time !
My question here is this connection correct, I am afraid to burn the board or the PC.
En the datasheet i understand that the board already generates 12V, but i am wondering how to connect the Peak lin (because i think they have to be connected to the same ground).