Question
Debug/programming another chip with STLINK from STM8disco
Posted on August 30, 2012 at 12:11
Hi,
After developping and testing with stm8s-discovery connected to various evalboards, i just received my prototype. As written in STM8SVLDISCOVERY's usermanual, i unsoldered the two 0 Ohms of swim connector from the STLINK (i don't want to break the discovery board yet). Now, i disconnected everything on my board (thru jumpers), except external power-supply to the micro, and i connected SWIM port and GND. The Chip i use is the STM8S105S4, and i already changed the device target. Using STVD/Cosmic, i try to enter debug mode and i receive this message :Starting debug session...
-> Emulator reset (usb://usb)...
** Connection error (usb://usb): swim error [30006]: comm init error: chip does not answer
-> Failed to connect target. Seeing SWIM_reset pin, i also connected it (althrough SWIM = SingleWire) and i get same message :\ What did i miss ?