Debug variables wrong
Hello,
I'm facing a very embarrasing problem with variables in ST visual develop.
When I add a breakpoint just before a function call and I hover the parameter being sent with my mouse I can see it. But when I step into the function, the parameter became wrong : it has totally random values.
Also when the mcu has to do calculations, it can do it wrong.
This kind of calculation can be wrong :
result = (uint16_t)((sqrt((float)sum / measures_nb) / 1023.0 * 3.3 / 0.1) * 1000);
If I do this with another compiler, the result is correct.
I disabled all optimisations except +split because without this I get a .text overflow
If someone can help, I appreciate.
Thanks