Question
delay_ms not working
I have copied the delay_ms function from the standard Discovery code, but I can't get it to work. It seems that it is running precise 10x too slow, so "delay_ms(100)" gives me a 1 sec delay.
Can anyone explain what is wrong?
/* MAIN.C file
*
* Copyright (c) 2002-2005 STMicroelectronics
*/
#include "stm8l15x.h"
/** DEFINES **/
#define GPIO_HIGH(a,b) a->ODR|=b
#define GPIO_LOW(a,b) a->ODR&=~b
#define GPIO_TOGGLE(a,b) a->ODR^=b
/** STM8L Discovery board **/
#define LED_BLUE_PORT GPIOC
#define LED_BLUE_PIN GPIO_Pin_7
/** LOCAL PROTOTYPES **/
void delay_ms(u16);
/******************************
* MAIN
*/
main()
{
GPIO_Init(LED_BLUE_PORT, LED_BLUE_PIN, GPIO_Mode_Out_PP_High_Fast);
GPIO_LOW(LED_BLUE_PORT, LED_BLUE_PIN);
while (1)
{
GPIO_HIGH(LED_BLUE_PORT, LED_BLUE_PIN);
delay_ms(100);
GPIO_LOW(LED_BLUE_PORT, LED_BLUE_PIN);
delay_ms(100);
}
}
/******************************
* DELAY_MS
*/
void delay_ms(u16 n_ms)
{
/* Init TIMER 4 */
CLK_PeripheralClockConfig(CLK_Peripheral_TIM4, ENABLE);
/* Init TIMER 4 prescaler: / (2^6) = /64 */
TIM4->PSCR = 6;
/* HSI div by 1 --> Auto-Reload value: 16M / 64 = 1/4M, 1/4M / 1k = 250*/
TIM4->ARR = 250;
/* Counter value: 2, to compensate the initialization of TIMER*/
TIM4->CNTR = 2;
/* clear update flag */
TIM4->SR1 &= ~TIM4_SR1_UIF;
/* Enable Counter */
TIM4->CR1 |= TIM4_CR1_CEN;
while(n_ms--)
{
while((TIM4->SR1 & TIM4_SR1_UIF) == 0) ;
TIM4->SR1 &= ~TIM4_SR1_UIF;
}
/* Disable Counter */
TIM4->CR1 &= ~TIM4_CR1_CEN;
}Thanks
Lars Bo Wassini