Skip to main content
Visitor II
August 17, 2017
Question

Dev boards for STM8 with plenty of RAM and for STM8A?

  • August 17, 2017
  • 1 reply
  • 638 views
Posted on August 17, 2017 at 21:26

It seems there are very few evaluation boards for the STM8A and for the cheap STM8 with lots of RAM. Basically the STMA-Discovery is the one notable exception.

I'd like to see more boards for the STM8A and for other STM8 that have at least 4K of RAM. The following STM8 variants seem to be particular interesting, but don't have evaluation boards yet (which means I could find neither ST nor third-party boards):

STM8AF6286 (the cheapest STM8AF with 6K of RAM)

STM8S007C6 (the cheapest STM8S with 6K of RAM)

STM8AL31E8A (the cheapest STM8AL with 4K of RAM)

STM8AF5268 (another relatively cheap STM8AF with 6K of RAM)

STM8S207K6 (another relatively cheap STM8S with 6K of RAM)

Does anyone know of boards for these (either already available or upcoming)?

Philipp

    This topic has been closed for replies.

    1 reply

    Graduate II
    August 17, 2017
    Posted on August 17, 2017 at 22:03

    Why don't you query the vendors of the currently available low cost boards? Or take one and replace the chip with one you prefer more?

    http://www.ebay.com/itm/STM8S105K4T6-STM8S-Development-Board-Module-Core-board-MCU-Learning-Board-/222516973122?hash=item33cf0b8e42:g:sm0AAOSwZKBZHx9h