"Error : Programming failed" while trying to program "STM8S103F3" microcontroller with "STVP"
I got a message "Error : Programming failed" while trying to program "STM8S103F3" microcontroller with "ST visual Programmer". Sometimes the microcontroller got programmed but several times it failed. I am using "ST-LINK V2" programmer (connections: - SWIM, RST, Ground, 3.3V) for it. I have connected a "1uF ceramic capacitor" to microcontroller's "VCAP" pin. What i observed in it that when microcontroller got programmed, the "SWIM" pin goes LOW from 3.3V. But when i got "Error : Programming failed" message at that time, the voltage on "SWIM" pin remains standstill at 3.3V.
So, please, anyone provide the solution for this problem. Thanks.
Message shown on STVP