Failed to start GDB.
I have been using ST Visual develop for months, with the same MCU: STM8L, compiling and debugging with no problem.
Then yesterday I started getting a message to say that it can't start GDB :
Starting debug session...
-> Failed to start GDB.(see also attached picture for message boxes).
I have checked that the file path is correct Tools->Options : Toolset
Tool set : STM8 Cosmic
Root path : C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8
I even tried uninstalling and re-installing, same error.
Occasionally I have seen a popup saying that there is a lack of memory - but there is plenty available.
I am running :
Windows 10
ST Visual develop (two version numbers given in the about box : 4.3.12, 3.6.5.2 Build 4 Aug 2017
#st-visual-develop #gdb