Halt mode and Current consumption
Hi,
I have a STM8S001J3. I want to put my uC in halt mode because I'm on battery. The problem is that halt mode consume around 1mA when the interrupts are enabled. I need interrupts to wake up from halt mode with my GPIO pin so I can't disable it.
I tried without the interrupts and the current consumption is around 4uA.
I can't imagine that interrupts consume so much and that this issue is mentionned nowhere in the documentations.
I join here a copy of my main function:
main()
{
GPIO_Init (LED, GPIO_MODE_OUT_PP_LOW_SLOW);
GPIO_Init (BT, GPIO_MODE_IN_PU_IT);
GPIO_Init (GPIOA, GPIO_PIN_3, GPIO_MODE_OUT_PP_LOW_SLOW);
GPIO_Init (GPIOD, GPIO_PIN_6, GPIO_MODE_OUT_PP_LOW_SLOW);
GPIO_WriteLow(GPIOA, GPIO_PIN_3);
GPIO_WriteLow(GPIOD, GPIO_PIN_6);
EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOB, EXTI_SENSITIVITY_RISE_ONLY);
enableInterrupts();
while (1)
{
if (bouton() && oneTime) //if button pressed
{
oneTime = 0;
if(sleep)
{
sleep = 0;
}
else
{
ledOff();
sleep = 1;
halt();
}
}
else if(!bouton() && !oneTime)
{
oneTime = 1;
}
}
}